3/31/2014 4:50 PM | |
Posts: 107 Rating: (2) |
i want to save some tags for know everytime the valor of that tags |
4/1/2014 8:36 AM | |
Posts: 107 Rating: (2) |
I want to save the value of tags, when I will restart the hmi the valuewill bethe same |
4/1/2014 9:09 AM | |
Joined: 2/6/2009 Last visit: 3/21/2024 Posts: 938 Rating: (118) |
Hi, We don't have to worry about saving the value If it is External Tag, since the values are saved in the PLC. If it is internal tag, You can use "Runtime Persistence" tag property on WinCC V7.0 onwards, If you have WinCC before V7.0 then write a script for saving the tag values to Text file using VB or C cript. Here is thel link forHow can you restore the values of internal tags after restarting WinCC Runtime? |
Last edited by: Saravana kumar at: 4/1/2014 9:13 AMLast edited by: Saravana kumar at: 4/1/2014 9:13 AM_______________________________________________________________ |
|
This contribution was helpful to1 thankful Users |
10/3/2014 3:44 PM | |
Posts: 10 Rating: (0) |
Hi, I need same, save some Tag values permanently, however there is no"Runtime Persistence" option at Tag properties? Thank you for the answer WinCC Advanced V13
|
10/9/2014 11:08 AM | |
Posts: 10 Rating: (0) |
UP |
Follow us on