10/7/2019 4:46 AM | |
Posts: 1 Rating: (0) |
Hi, I'm also having time syncing issues. I have a Central HM, 5 local OS and 5 corresponding PLCs all on the same LAN. The central HMI allows to view the screens from each local OS. Each OS is set to get time sync from the CentralHMI using "get time from specific computer" option under time synchronization in WinCC. Each PLC is set as slave. But the time synchronization is not working. Its as if the central HMI is not broadcasting the time signal. I've checked and CCTMTimeSync.exe is set to start with winCC. Any ideas please? How can I test that the CentralHMI is actually broadcasting? I note that the "Process controlling messages.. send once" tick box is ticked. Should this not be ticked and a suitable time interval be set? Really driving me mad now! ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 10/07/2019 15:46:34New subject after splitting |
|
10/29/2019 1:13 PM | |
Joined: 12/12/2011 Last visit: 12/30/2020 Posts: 821 Rating: (39)
|
Hi, if i were you i would check this: https://support.industry.siemens.com/cs/ww/en/view/86535497 B.R. |
Grundkurs/Systemkurs WinCC V7: |
|
Follow us on