8/7/2019 3:07 PM | |
Posts: 5 Rating: (0) |
Hello, Can I test the electronics applying the P24, P5, P15 and N15 voltages? |
8/7/2019 3:16 PM | |
Joined: 7/19/2013 Last visit: 11/15/2023 Posts: 24 Rating: (0) |
what is the MLFB type number? photo? |
8/7/2019 3:48 PM | |
Posts: 5 Rating: (0) |
That is my control unit. |
8/7/2019 4:29 PM | |
Joined: 7/19/2013 Last visit: 11/15/2023 Posts: 24 Rating: (0) |
Check with multimeter and connection diagram chapter 2.3 of manual https://support.industry.siemens.com/cs/ch/en/view/103598510 is there a fault? |
Last edited by: Jen_Moderator at: 08/08/2019 09:24:48Optimized link. |
|
8/7/2019 6:40 PM | |
Posts: 5 Rating: (0) |
There is no fault. I tried to change the board. The one I put in place of the one in the picture, called. The other not. I know she needs a voltage of 57V at 20kHz to work. My question would be if there is a possibility to connect it using only the voltage pins, P5, P15, N15 and P24. Do you know if there's any way I can do this? AttachmentRIBBON_CABLE_DATA.pdf (745 Downloads) |
Last edited by: TMarp at: 08/07/2019 18:41:38 |
|
8/8/2019 2:01 PM | |
Joined: 7/19/2013 Last visit: 11/15/2023 Posts: 24 Rating: (0) |
Dont know, sorry. |
8/9/2019 3:15 PM | |
Posts: 5 Rating: (0) |
Okay. But, how can I test it? Can I test it using the E/R modul? |
8/10/2019 9:04 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Yes, you can test it with ER module plus appropriate motor set up. |
Follow us on