9/21/2017 1:13 PM | |
Joined: 11/5/2016 Last visit: 5/2/2024 Posts: 9 Rating: (0) |
Hi all, This is Kaustubh, M using S7 1200 CM1241 RS232 module for communication with epson printer, The printer communication settings are like this.. Baud-9600bps, Parity-none, Data bits-8 bits, Stop bits - NA, Parallel I/F Bidirectional mode-On Packet Mode - Auto We previously had a succefull print from Siemens Smart ST30 (from CM01 module in free port mode)plc on this printer CAN SUMBDY PLZ TEL ME HOE TO DO THIS PRINT FROM CM1241 OF S7 1200. I tried instruction "port_config" and after this "send_ptp" but printer is not even moving. is der any method by which should i give command & texts for printing on printer. Please help.....! Thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 9/21/2017 2:04:13 PMNew subject after splitting |
|
Follow us on