11/17/2021 12:02 PM | |
Joined: 12/17/2020 Last visit: 4/16/2024 Posts: 14 Rating: (0) |
Hi, i'm using a MTP1500 Unified Confort panel. I have created 2 users and download the software into my panel and works fine. I have created a button with the "LogOff" function, but it does not work on the panel, but works only in simulation (with Google Crome). How I can manage the log-in / LogOff on the panel Runtime ? I'm using Tia v17 Thanks
------------------------------------------------------------------------------------------ |
Last edited by: Elia_Longoni at: 11/17/2021 12:02:44Last edited by: Elia_Longoni at: 11/17/2021 12:23:59Last edited by: Jen_Moderator at: 11/18/2021 14:06:23New subject after splitting |
|
11/19/2021 8:57 AM | |
Joined: 2/13/2020 Last visit: 1/28/2023 Posts: 54 Rating: (10) |
Hi Elia In the panels you aren´t promted for log in before you execute a function you are not permitted. On my LogOff button I have an authorization that all my users have in common, that way I am promted for a LogIn when no user is logged on and can log off with the same button no matter which user is logged on.
|
This contribution was helpful to1 thankful Users |
11/19/2021 11:26 AM | |
Joined: 12/17/2020 Last visit: 4/16/2024 Posts: 14 Rating: (0) |
Hi Stefán, I have created a User-specific right on my LogOff button and now it works also in the Unified panel. Thanks. I have another question: why when I log-off the user, the variable @Username still show the previous login user?
|
Follow us on