8/7/2019 11:14 AM | |
Posts: 28 Rating: (0) |
I think I managed to solve this problem. However, my program will have to be done in FC then in main call the functions I want. I leave a print of how the project is currently. My question now is how in Main I will call the functions sequentially, for example, call the reset block, then the read block, wait a few seconds, then call the write block, etc.. Best regards ------------------------------------------------------------------------------------------ |
Last edited by: CarlosInacio at: 08/07/2019 11:22:25Last edited by: Jen_Moderator at: 08/07/2019 11:59:02New subject after splitting |
|
8/7/2019 4:50 PM | |
Joined: 10/1/2013 Last visit: 4/17/2024 Posts: 605 Rating: (71)
|
All you have to do is to work with the block outputs. For example: IF reset.done THEN read.execute := TRUE; END IF; IF read.done THEN write.execute := TRUE; END IF; IF write.done THEN read.execute := TRUE; END IF; In this example continuous read and write operations are processed after a reset. There's no limit to your creativity. Additionally I suggest having a training for SCL programing because your question is a common question on how to programming instead of RFID related. https://new.siemens.com/global/en/products/services/industry/sitrain.html#countryselector |
Follow us on