11/2/2010 11:27 AM | |
Posts: 20 Rating: (0) |
I have second question in this theard. How conecting two S7-1200 with one panel basic ktp1000. I know this is passible but I don't kow how. Someone have any examples? Thanks for yours replay. Splitted from Can I conect two ktp panels with one cpu?. |
Last edited by: O_Moderator at: 11/2/2010 11:38 AMnew subject after splitting |
|
11/2/2010 11:58 AM | |
Joined: 4/24/2006 Last visit: 4/25/2024 Posts: 8613 Rating: (1147)
|
Dear e-kuba, Can you mention which Software you use? Best regards, Wizard |
11/2/2010 5:36 PM | |
Posts: 20 Rating: (0) |
STEP 7 BASIC V10.5 |
11/3/2010 9:23 AM | |
Joined: 4/24/2006 Last visit: 4/25/2024 Posts: 8613 Rating: (1147)
|
Dear e-kuba, When you start Step 7 Basic (TIA), you will have here 1x basic panel KTP1000 and 2x CPU S7-1200. When you go to "Devices & Networks", you can select the HMI and with right mouse click, go to "Create new connection" Now it is possible to select the desired CPU. And perhaps this link, might help to determine the maximum number of connections: What is the maximum number of simultaneously active controller connections you can configure for a panel? Best regards, Wizard |
11/3/2010 11:11 PM | |
Posts: 20 Rating: (0) |
Thank you very much! |
12/30/2010 1:52 AM | |
Posts: 7 Rating: (0) |
Hi, I tried to do what you explain to establish the comm between two plc and one KTP but i'm not able to find where is the ADD NEW CONNECTION. I include a print screen. I'm using V10.5 sp2 update1 Regards AttachmentDoc1.pdf (88 Downloads) |
12/30/2010 9:33 PM | |
Posts: 7 Rating: (0) |
thank a lot i found how to make it Best regards |
This contribution was helpful to1 thankful Users |
Follow us on