3/1/2013 4:50 PM | |
Posts: 13 Rating: (0) |
hello all, plz help i want to convert a word to int , for (==I) test ??? |
3/1/2013 4:56 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365)
|
Hello , Please give us more information on your "WORD" variable. How data stored in that variable.Is it like "BCD"?If it is not "BCD", it can be considered as an INT without any change. If you are using LAD,For comparison you should Un-check type check in LAD/STL/FBD editor(type_check.jpg ). Best regards Hamid Hosseini |
Last edited by: hdhosseini at: 3/1/2013 4:58 PM |
|
3/1/2013 5:13 PM | |
Posts: 13 Rating: (0) |
thankx brother, i want to compare a out counter Z_vorw with his PV, the probleme is operande ==I dont work good with 2 word i think?? no? |
3/1/2013 6:27 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365)
|
Hello , I remember same discussion before here. Compare Arrays of Chars
For that reason I do agree with idea of my friend "fritz". Best regards Hamid Hosseini |
This contribution was helpful to2 thankful Users |
3/2/2013 4:51 PM | |
Joined: 4/20/2007 Last visit: 9/19/2024 Posts: 727 Rating: (42) |
Tarik, You probably have run into a BCD conversion error. Lookherefor an example. Basicly, you are probably trying to convert a number from BCD to INT somewhere. |
Follow us on