Industry Online Support
Technical Forum
8/17/2012 8:10 PM | |
Posts: 13 Rating: (0) |
Hi all, I have a Text Field that has it's visibility linked to a DB in the PLC. I have 16 of these DBs, and I want each one tagged to the same visibility property in the one Text Field. I've looked at the following chart (pdf-attachment in the following entry): http://support.automation.siemens.com/WW/view/en/53752382 I see there is a Visible option, but it is linked only to a boolean value. Do you guys know of a way to go even further with vbscript and define the Tag associated with that visibility propterty? Below is where I am so far.. Thanks 'Text Field_40 Set TextField_40 = HmiRuntime.Screens("FACS\OO_237_ErrorProofingTask_1B").ScreenItems("Text Field_40") If SmartTags("FACS\Proof_SelectionTag") = 1 Then TextField_40.Visible = SmartTags("FACS\Vision_1_Sub_1").Value ElseIf SmartTags("FACS\Proof_SelectionTag") = 2 Then TextField_40.Visible = SmartTags("FACS\Vision_2_Sub_1").Value ElseIf SmartTags("FACS\Proof_SelectionTag") = 3 Then TextField_40.Visible = SmartTags("FACS\Vision_3_Sub_1").Value ElseIf SmartTags("FACS\Proof_SelectionTag") = 4 Then TextField_40.Visible = SmartTags("FACS\Vision_4_Sub_1").Value Else 'Do Nothing End If |
Last edited by: O_Moderator at: 8/20/2012 9:25 AMlink corrected Last edited by: flylikechris at: 8/17/2012 8:15 PM |
|
Follow us on