11/27/2018 11:25 AM | |
Joined: 9/30/2016 Last visit: 4/5/2024 Posts: 910 Rating: (6) |
Hi while(1<2), Thanks you again. I can correct the name in WinCC Server - but HOW do I do this: "After that create the Server Data newly in the server project."?
|
11/28/2018 8:23 AM | |
Joined: 9/30/2016 Last visit: 4/5/2024 Posts: 910 Rating: (6) |
Hi again while(1<2), The WinCC client I am replacing is version 7.0 SP3 Upd.1. And the plan was to keep it is this version since the server it is connected to is in that version. IS it best that the client has the same version as the server or are they (fully) independent version-vise? I have WinCC 7.4 SP1 RC on my "personal" work laptop but I cannot use that as an ES due because this PC is also on the company network (not "just" the control network) and is therefore too limited in the user rights. I do not need a redundant server - so why would we test that? I can use the Project Duplicator and make a copy of the project - but is it OK to use my WinCC 7.4 SP to do it (or will it be updated from 7.0 to 7.4 if I do that? Could I perhaps do this with the WinCC 7.0 Sp3 Upd1 Client when the software has been installed? How do I test if I can create the server data in the "Saved As..." project? Is that by right-clicking an choosing "configure"? Also - which options do I pick (which boxes in the screenshots do I check) to make a functional replacement of the client?
AttachmentWCCC.zip (50 Downloads) |
Last edited by: xmnj at: 11/28/2018 9:28:11 AM |
|
Follow us on