4/29/2019 9:06 AM | |
Joined: 9/30/2016 Last visit: 8/15/2024 Posts: 914 Rating: (6) |
Please also see the screenshots. I need to be able to show a single paged pfd document as a display. I have found out I can use the WinCCWebBrowser object and that works fine. But I would really like to just show the page and not show any menus around the page - how do I do that? Or is there another way (instead of the WinCCWebBrowser object) of displaying a single pdf page? As a second choice If I cannot remove the menu with the control buttons I could also settle for blocking the buttons from working - how do I do this? AttachmentDiv 3.zip (36 Downloads) |
Last edited by: xmnj at: 04/29/2019 09:38:17Clarification |
|
4/29/2019 9:57 AM | |
Joined: 9/19/2009 Last visit: 9/14/2024 Posts: 459 Rating: (85) |
Hi You have severals options to show a pdf file. As you said, you have WinCCWebBrowser, if you install Acrobat Reader, you will have another ActiveX , another choice is Foxit Reader. This have the following Active X FoxitReaderBrowserAx.dll and I´m sure there is more ActiveX With WinCCWebBrowser you can disable the navigation tool bar. It is spanish but take a look to this sample. Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
4/29/2019 10:26 AM | |
Joined: 9/30/2016 Last visit: 8/15/2024 Posts: 914 Rating: (6) |
Thank you for answering Georg. That is a good option - if I can find out where the picture window is located in the objects menu (even though switching them off would be more "elegant" than "simply covering them" it should still work.
Thank you for answering *PHS*. I am not really interested in installing any more software than I have to - so would prefer to stay with the WinCCWebBrowser. If you look at my screenshots in the original post you will notice I have disabled all the options I have - or am I looking in the wrong places?
|
Follow us on