8/16/2018 11:22 AM | |
Joined: 2/11/2015 Last visit: 9/19/2024 Posts: 464 Rating: (34) |
Hi, Maybe this helps you... Do the first row for each color |
8/16/2018 1:15 PM | |
Joined: 9/30/2016 Last visit: 8/15/2024 Posts: 914 Rating: (6) |
Thank you Wizard, Please also see the attached screenshots. I have made an input and an output (both of the type word) and some Boolean temporary variables in the block interface. I CAN connect DB501.DBW458 to the input pin but I cannot connect DB1208.DBW0 to the output. What is wrong and how do I correct it? Also - I have made some logic that should work but I would like to make it more "elegant" as it is pretty "clunky" - any suggestions? AttachmentFC.1210.zip (183 Downloads) |
8/16/2018 1:23 PM | |
Joined: 4/24/2006 Last visit: 9/20/2024 Posts: 8742 Rating: (1168) |
Hello, Please check the datatype of DB1208.DBW0 Best regards, Wizard |
8/16/2018 1:41 PM | |
Joined: 4/24/2006 Last visit: 9/20/2024 Posts: 8742 Rating: (1168) |
Hi, I think that is the problem. Change datatype in DB to Word. Best regards, Wizard |
Follow us on