9/3/2020 9:32 AM | |
Joined: 9/30/2016 Last visit: 4/5/2024 Posts: 910 Rating: (6) |
Please see the attached screenshots. I have a WinCC 7.0 computer (which is no longer connected to the PLC) that I need to get some logged values from. I have made a Trend display with the values I was and set it up to show the time period I am interested in. Now I want to export the numbers in a CSV file so I can work with them in Excel and i THINK I set up the eksport tab correctly - but it is not creating any file. What do I need to do to get a CSV file with the logged values? AttachmentFB1 KIC logs A.zip (44 Downloads) |
Follow us on