12/6/2018 1:40 PM | |
Joined: 9/30/2016 Last visit: 8/15/2024 Posts: 914 Rating: (6) |
Please also see the attached screenshots. We are using STARTER vie Simatic Manager to program our Siemens G120 Drives. I would like to make a comparison between an older program and the current. How can I do this? I am imagining to export old and new program to Excel and compare them with Excel but it would be great if it could be done in STARTER without needing to export. Can it be done locally and if so HOW? I have tried to export the program but I am just getting the error message "" and a message stating that Export is not possible. What am I doing wrong and how should I do it to make it work? AttachmentStarter.zip (261 Downloads) |
12/7/2018 11:43 AM | |
Joined: 9/30/2016 Last visit: 8/15/2024 Posts: 914 Rating: (6) |
Thank you ChristophD, Yes - that way the export can be done. I am not sure what I can read in the resulting xml file but that is for another thread :-D |
Follow us on