3/19/2019 9:25 AM | |
Joined: 9/30/2016 Last visit: 8/15/2024 Posts: 914 Rating: (6) |
Please also see the attached screenshots. I have 2 Schmersal proximity sensors wired to 2 channels in a F-DI module (6ES7 326-1BK02-0AB0). This happens the same way in both left and right sides (so 4 channels and 4 sensors are used). Each of the proximity sensors has 2 switches and these are wired "to cross each other" in a way that I18.4 and I18.5 both are activated when both sensors are activated and none of them are activated when no sensor are activated. However - I am experiencing that I only get either I18.4 or I18.5 even though both sensors are activated. I am thinking it can be because of the discrepancy time is set to 10 ms on I18.4 and I18.6 to 20 on I18.5 and not at all on I18.7. I would like to set them all to 50 or 100 ms - how do I do that (also I18.7 which seems not to set up for discrepancy time)? Attachment18136.zip (175 Downloads) |
Follow us on