5/13/2020 12:56 PM | |
Joined: 9/30/2016 Last visit: 8/15/2024 Posts: 914 Rating: (6) |
Please see attached screenshots. I am replacing one FB with another FB in Network 5. I have deleted the "old" FB so the output from the first and gate (and several more) is not connected anymore (shown in the first screenshot). Now I want to connect it to the "Stanstill-pin" on FB101 (shown in the second screenshot). How do I do this - I have tried drawing the mouse and double clicking but that does not seem to work? AttachmentEB5 FB101 B.zip (68 Downloads) |
Follow us on