12/18/2018 7:38 AM | |
Joined: 9/30/2016 Last visit: 8/15/2024 Posts: 914 Rating: (6) |
Hi Hati, Thank you for answering. The numbers are coming from the PLC. Each number is a status DBW for a gear lever, The status and position of the levers are shown in the main HMI (WinCC 7.4 SP1) as a square that can be the mentioned 4 colors. In WinCC 7.4 SP1 the square is a faceplate which does the masking so the DBW can be connected directly to the faceplate. I need to show the same status In the basic panel but basic panels do not support faceplates and I would not have the correct faceplate anyway. I guess I will have to make the logic in the PLC. It is a simpler since the color I need only depends on 2 of the bits in the DBW as the screenshots show.
Attachmentdectobin.zip (32 Downloads) |
Follow us on