10/15/2013 7:13 PM | |
Joined: 7/7/2010 Last visit: 5/10/2024 Posts: 14709 Rating: (2356)
|
You might try an undelete program. In the meantime, you might want to purchase another memory card. Maybe a recovery program like testdisk ( http://www.cgsecurity.org/wiki/TestDisk). Scan software before using as you would any unknown source. |
science guy |
|
This contribution was helpful to1 thankful Users |
11/6/2013 11:08 AM | |
Joined: 1/23/2009 Last visit: 11/3/2022 Posts: 29 Rating: (10) |
Try to copy crdinfo and LOG files to memory card. I put this files in attachments... I copy this files from Simatic 24MB memory cards Best regards AttachmentCrdinfo & LOG.zip (987 Downloads) |
Be creative while inventing ideas and be disciplined while implementing them... :) |
|
This contribution was helpful to1 thankful Users |
11/10/2013 10:55 PM | |||||||||
Posts: 58 Rating: (10) |
What's the problem, for the 1200 you just have to insert the SMC to get the files back. (Assuming in 2013 you don't have a firmware < V2.0.1) http://support.automation.siemens.com/WW/view/en/69063975 Restoring the memory card with S7-1200
Note |
||||||||
This contribution was helpful to1 thankful Users |
12/8/2016 10:54 AM | |
Posts: 2 Rating: (0) |
Insert memory card in card reader and connect it with PC. Note down the hard drive name. for example if your card is showing as D: drive then you have to enter d: in the command prompt. Now click Start and in search bar type in ‘cmd’ and hit Enter After this the command prompt window will open. Now type in"attrib -s -h /s /d *.*”(or)“attrib -h -s -r /s /d *.*” Now open your memory card and you will find the hidden files. Source - http://www.rescuedigitalmedia.com/solved-recover-hidden-media-files-memory-card |