7/30/2021 11:40 AM | |
Joined: 9/30/2016 Last visit: 8/15/2024 Posts: 914 Rating: (6) |
Please also see the attached screenshots. I have a machine where I expected the HW configuration had not been saved in our AsBuilt system after a minor modification. I open the HW configuration and when I want to go online I am (as expected)t old that there is a difference between offline and online and offered to upload the HW config from the PLC to the PG. I accept this and see that some copying takes place. I expect the offline and online (PG and PLC) HW config have been synchronized to that which is running in the PLC. However when I open the online view again I am AGAIN informed that there is a difference and offered to copy. So - how do I synchronize the offline and online (PG and PLC) HW config to that which is running in the PLC CORRECTLY - so that I am not "running in circles"? I also tried to pick the copy option while in offline view (pic 4 & 5) and I selected the project the offline files are in but I did not know what to select under the node address? AttachmentGB536 A.zip (386 Downloads) |