2/8/2018 1:23 PM | |
Joined: 6/5/2011 Last visit: 8/29/2024 Posts: 5 Rating: (0) |
Dear All, I am using TP1200 comfort, i want to write a csv file to shared folder in a PC (OS is Window 10). My shared folder setting: Advanced Sharing - Permissions - Everyone - Full Control (Allow) ; Change (Allow) ; Read (Allow) But still could't write the CSV file. Please Help, is it possible to integrate TP1200 into a local network with windows 10 ? as i can see in this link below, it only mention windows 7 (I already try my script with windows 7 and it work well). https://support.industry.siemens.com/cs/nl/en/view/13336639 Best regards, Erick |
Last edited by: l_p at: 2/8/2018 1:54:28 PMLast edited by: Jen_Moderator at: 2/8/2018 2:00:47 PMOptimized link. |
|
2/11/2018 1:37 AM | |
Joined: 10/25/2016 Last visit: 9/1/2022 Posts: 199 Rating: (25) |
Hi Erik, If you can't, try using a virtual machine Regards |
2/22/2018 4:21 PM | |
Joined: 8/3/2009 Last visit: 9/24/2024 Posts: 13778 Rating: (1740)
|
Hello I_p You cannot use "everyone" in the share settings on the PC. You have to create a local user on the PC who has the rights for the share. Then on the Panel at settings-> network ID you have to enter the same settings. It will not work if you use everyone. And of course you should use this FAQ: https://support.industry.siemens.com/cs/ww/en/view/92346478 Bye Murof |
Last edited by: Murof at: 2/22/2018 4:22:08 PMIf this Information really helps, you could use the Rate function |
|
11/3/2018 4:34 PM | |
Joined: 4/19/2018 Last visit: 8/23/2024 Posts: 2 Rating: (0) |
Hi! You must enable SMB1.0 on windows 10 "windows features" -T |
This contribution was helpful to1 thankful Users |
Follow us on