7/26/2009 10:06 PM | |
Posts: 43 Rating: (0) |
hello how i can communicate with micoms and drise in the field? i want to know the methods in details or i need any helpful documents thanks |
7/31/2009 1:24 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, Give us what exactly model of MICOM you have. ( http://www.areva-td.com/solutions/US_366_Solution+Index.html ). Basicaly most of this device supports Modbus and IEC 61850 (with optional Ethernet port). But if you have options "cards" you can "take" other possibilities. Also the simpler devices has inbuild analog ouputs which you can use directly connected to AI into PLC. About "drise" (this is very common name). But the logic is the same. Regards, Hristo Mihalev |