7/7/2010 12:32 PM | |
Joined: 9/23/2005 Last visit: 4/17/2024 Posts: 4325 Rating: (1419) |
Hi, I think that this information is more useful that all other, because with this, the customers could found your particular solutions by himself. So, I wrote this TIP. Attachmentany.pdf (5621 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to11 thankful Users |
7/7/2010 1:55 PM | |
Joined: 7/2/2008 Last visit: 4/5/2024 Posts: 928 Rating: (305) |
Hello Pegaia, 1-Thank you for sharing information and knowledge. 2-It's very niceto have your tips back in field ofSTEP7 since you have been quite busy with S7-1200 and STEP 7 Basic. 3- I think the attachment shows the same but in another way of representation. The attachment has been extracted froma very precious document called Programming with STEP 7 V5.4. Best regards. H-H AttachmentANY pointer.pdf (3013 Downloads) |
This contribution was helpful to2 thankful Users |
7/8/2010 11:02 AM | |
Joined: 10/7/2005 Last visit: 4/18/2024 Posts: 3003 Rating: (1046)
|
H-H's pdf is also my preferred reference for ANY pointer structure and it is also part of the inbuilt Step 7 help and as such quicklyavailable in times of need (type in ANY as a keyword in the index search field). EDIT: My entry looks "empty" now that the rest of my answer was cut out from here and split into THIS thread. On the bright side, it gives me another chance to point people to THIS thread to hopefully revive it and perhapsgetsome answers |
Last edited by: fritz at: 7/8/2010 11:40 AMAdded "EDIT" entry Last edited by: O_Moderator at: 7/8/2010 11:25 AMCheers |
|
This contribution was helpful to1 thankful Users |
6/22/2012 5:20 PM | |
Joined: 10/24/2011 Last visit: 3/9/2023 Posts: 257 Rating: (1) |
Hi Pegaia, Thanks..PDF is very nicely explained.. Thanks for support.. Shailesh |
Follow us on