11/6/2014 9:46 AM | |
Posts: 49 Rating: (1) |
dear all, In short, how many PLC S71200 connect to Wincc 7.2? For example, if i use IE or CP, how many PLC? Any licence for it.
------------------- New subject after splitting from Simatic WinCC 7.2 maximum number of connections to S7-1200 CPU. |
Last edited by: Min_Moderator at: 11/6/2014 12:13 PMSplitted |
|
11/6/2014 3:11 PM | |
Posts: 1058 Rating: (93) |
Hello SIS AN, as far as I know you can connect a maximum of 32 S7 1200 CPUs to WinCC 7.2, but in reality you will be limited by the power of WINCC. At some point it will be too slow. regards |
12/5/2014 4:07 AM | |
Posts: 49 Rating: (1) |
Dear Sir, How many PLC S7 can connect Wincc 7.2 via IE ethernet? and How many for CP ethernet card?
|
12/5/2014 10:30 AM | |
Posts: 1058 Rating: (93) |
Hello SIS AN, maximum connections of 32 applies to WinCC 7.2, no matter how you connect. see Technical Data WinCC V7.2 regards |
12/5/2014 7:09 PM | |
Posts: 49 Rating: (1) |
dearbg2492, If you use a Workstation-OS like Windows 7, you have a limmitation to 8 connections, this case i must buy licence Sofnet Lean. Is it right? with a Server-OS you can have up to 60 connections. this case, i must buy licence Sofnet Full, is it ok? With a CP you do not have this limmitation with the Workstation-OS. I only buy licence hardnet. Is it ok? HElp me, when do you buy licence Softnet ? When for hardnet? To me, hardnet for CP and sofnet for IE ethernet. Thanks
|
12/8/2014 11:05 AM | |
Posts: 49 Rating: (1) |
dearbg2492, I said that sofnet licence is for IE card and Hardnet for CP card. But i read the manual( as i attach), -Sofnet is for CP 1612-A2 and not for IE card . - hardnet is for CP 1613-A2, CP 1623, CP 1628. Could you explain clearly about this problem.? Thks
Attachmentsimatic_st80_stpc_complete_english_2013.pdf (263 Downloads) |
12/8/2014 12:53 PM | |
Posts: 49 Rating: (1) |
dearbg2492, 1.I don't really understand clearly about difference between hardnet and sofnet licence. Give me more detail such as manual,.. 2. If i use IE card( onboard). How many connecctions i can? Is it 8 connections? Any licence for this case? Thanks alot
|
Follow us on