8/21/2017 6:50 AM | |
Joined: 9/11/2012 Last visit: 3/30/2023 Posts: 70 Rating: (5) |
Dear Tilu, Which interlock you want to add? please share you HMI program (faceplate screen) with PLC backup. |
If this post helped you, you may use the Rate-button |
|
8/21/2017 7:51 AM | |
Posts: 44 Rating: (0) |
Dear Atul ji, plz find the faceplate image. |
8/21/2017 8:47 AM | |
Joined: 9/11/2012 Last visit: 3/30/2023 Posts: 70 Rating: (5) |
Share your PLC backup and HMI program. Only screen shoot is not more clear to understand. |
If this post helped you, you may use the Rate-button |
|
8/21/2017 11:12 AM | |
Posts: 44 Rating: (0) |
Dear Atul ji, pls find the program backup. I want to add extra interlock in TT3 chart. But in TT3 only 8 interlocks. Right now i have no hmi backup,i will arrange soon. AttachmentOhp_rm.zip (62 Downloads) |
8/21/2017 11:33 AM | |
Joined: 9/11/2012 Last visit: 3/30/2023 Posts: 70 Rating: (5) |
Unfortunately, your all three blocks have been locked.
|
If this post helped you, you may use the Rate-button |
|
8/21/2017 12:37 PM | |
Posts: 44 Rating: (0) |
Dear Atul ji, Can i add Intlk4 block for this?? But all interlocks should be shown in one faceplate. |
8/22/2017 4:50 AM | |
Joined: 9/9/2015 Last visit: 9/15/2024 Posts: 727 Rating: (278) |
Dear Tilu, In this case, you would need the source file of your customized interlock block. Then you have two options to do it, 1. edit the source file, expand the input to 3 more extras. Then modify your faceplate. 2. create another function block with a new name, reuse your source file and add three more inputs for it. Then modify your faceplate. Hope this helps. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
8/22/2017 9:53 AM | |
Joined: 9/11/2012 Last visit: 3/30/2023 Posts: 70 Rating: (5) |
Share your complete backup (PLC and HMI). I will check and confirm if possible to add interlocks as well as in HMI faceplate also. |
If this post helped you, you may use the Rate-button |
|
8/23/2017 12:01 PM | |
Posts: 44 Rating: (0) |
Dear Atul ji, Right now I have take 16 intlk block and made the interlock connection in chart,then delete 8 intlk block from chart.Compile and Download both chart & hmi.Its faceplate also shown in HMI with extra added interlock. Tilu |
Follow us on