2/7/2018 3:29 PM | |
Joined: 6/30/2014 Last visit: 4/17/2024 Posts: 456 Rating: (86)
|
Dear COMOS Admins and super users, Maybe you have the task to implement own (documentation) files to the the COMOS help. You may find how to do that in the official ReadMe-File, which Siemens delivers with COMOS: "7.2 Copying documentation to the help folder Requirement COMOS is installed. Permissible data types: .doc / .docx / .txt / .pdf Procedure 1. Open the directory in which the help files are located in the file explorer. For example: <COMOS installation directory>/Help/<Language folder>. 2. Save your documentation in the <Language folder>. Note "Help" directory Documents that are located directly in the "Help" directory are not displayed. Result The files are displayed in COMOS with the "Help" button." If you like, have a look into the attached file, as I did. Please feel free to share your experiences, also about this point, with us all here. ====> As far I can see, this still works fine (I can also see it in the documentation) with COMOS 10.2.4 With best regards, SuperPippo AttachmentCOMOS_Readme_10.2.2-Page 46.pdf (478 Downloads) |
Last edited by: SuperPippo at: 1/9/2019 8:20:24 AM |
|
This contribution was helpful to2 thankful Users |
Follow us on