Industry Online Support
Technical Forum
8/21/2013 8:13 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306) |
i would be thankful for your help :) Hi ahabala SIPROTEC-4 relays support many different communication Protocols ( Depending upto the MLFB No ) . e.g. a) PROFIBUS-DP b) PROFIBUS-FMS c) Modbus d) IEC-60870-5-103 e) IEC-61850 etc. The Hardware / Software required to connect the relay will vary based on the same. Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
This contribution was helpful to1 thankful Users |
Follow us on