Industry Online Support
Technical Forum
9/6/2010 7:06 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181)
|
Hello Hammad Riaz, 1. Prosave' Complete backup can't be edit. Only to restore on the same type of panel. 2. To take backup using Protool is possible only, if the Transfer of the current project file from the configuration computer to the operating unit must be performed using the Upload option "Enable upload". Look at Back_transfer_description_e.pdf There have explanation what are possible remedies there. Best regards, Hristo Mihalev |
9/7/2010 8:04 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181)
|
Hello Hammad Riaz, About "*.pdz file is not found" loook at the link in my previous post. About old version of Protool look at Open Pro Tool 1.x configuration with current software . I suggest you to contact with Siemenes Hotline. Best regards, Hristo Mihalev |