3/5/2019 1:49 AM | |
Joined: 4/4/2016 Last visit: 1/14/2020 Posts: 52 Rating: (1) |
Hi, I am using node-red to commnunicate with LOGO8 and i woud like to know if there is a way to change the Hour and Minute in the Weekly timer Block ? I have mapped the parameter On Time and on the node-red side i can write in the VM , the value changes but the format does not match. Any possible help ? Regards, MD ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/5/2019 7:39:23 AMNew subject after splitting |
|
3/6/2019 2:34 PM | |
Joined: 4/4/2016 Last visit: 1/14/2020 Posts: 52 Rating: (1) |
Attached simple flow i am using for testing. Thanks Regards, MD AttachmentConvertHexToDecimal.txt (663 Downloads) |
3/8/2019 10:34 AM | |
Joined: 4/28/2015 Last visit: 3/23/2024 Posts: 3345 Rating: (377)
|
Hi, I cannot find any code which can "translate" Hex/Dec into BCD. But there is a node: https://flows.nodered.org/node/node-red-contrib-binary I will try that.. Not sure yet if this is the right functionality you are searching for. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
3/9/2019 12:19 AM | |
Joined: 4/4/2016 Last visit: 1/14/2020 Posts: 52 Rating: (1) |
Hi, I have already tried the node you mention but does not work. I think the solution could be use a function block node in node-red to write a script to convert the input Hex to output Decimal based on the calculation Scorp has described. Regards MD |
Follow us on