3/29/2016 9:04 AM | |
Posts: 7 Rating: (0) |
Hello I will try to describe it more - the screenshots are available in the annex as a single pdf file ( numbers in the post, are connected with those in the pdf file). 1. I want to change value of local variables using buttons. 2. If the command is correct, I want via script in VB rewrite the state of local variables on the variables avalible in the properties. 3. View variables from properties. I hope that now everything is clear. Best regards Mikolaj AttachmentWinCC_Properties.pdf (374 Downloads) |
3/29/2016 2:13 PM | |
Posts: 7 Rating: (0) |
Yes, I'm using faceplates for WinCC RT Advanced/Comfort Panel - TIA Portal V13 Sp1 Up7. I have a problem with changing values of variables in properties by using scripts in VB. Step 2. When I'm using syntax like you showed me, complier throws an error. I pu a second pdf file. 1. The name of the script in VB with syntax and command. 2. Way to run the script ( click button). 3. Error when compiling P.S. I'm using the same syntax as you. AttachmentWinCC_Propertiess_2.pdf (292 Downloads) |
Follow us on