12/17/2008 11:04 AM | |
Joined: 9/7/2007 Last visit: 8/30/2023 Posts: 550 Rating: (62) |
Hi, You can get from the technical specification of each components the Current consumption and there will be all the data you need https://mall.automation.siemens.com/gb/guest/index.asp?caller=CA01&Lang=en&nodeid=10017499 Best Regards |
Best Regards |
|
12/18/2008 11:36 AM | |
Posts: 217 Rating: (52) |
Dear how come, I think that means the deference between total power in and total power out. Total power in = Total power consumption + Power loss. I think this may help you. Thanks. |
12/19/2008 7:34 AM | |
Posts: 382 Rating: (47) |
Dear Arunakat1, with regards, how come? |
12/20/2008 4:13 AM | |
Posts: 217 Rating: (52) |
Dear how come, IthinkitisindicatinginxxxmAbecauseitiseasertochoosewhichpowersupplyyouaregoingto use. For example if you use 10 modules of 100mA and 20nos of 200mA coils (solenoids, contactors etc). For modules its 10*100mA = 1000mA=1A and for coils its 20*200mA= 4000mA= 4A So you have to use at least 4A+1A =5A Power supply I hope this will help you. Thanks |
12/23/2008 2:29 AM | |
Posts: 382 Rating: (47) |
Dear Arunakat1, In this case if i want to obtain the power consumption in "watt", what should i do? Thanks in advance! |
12/23/2008 4:16 AM | |
Posts: 217 Rating: (52) |
Dear how come, I think it’s easy if you want to go with watt you jest use this formula P=VI cosf where P power in watts V voltage in volts I current in Amps In DC cosf will be 0. So if you know the current and voltage you can easily calculate the power in watts. I hope this will help you. Thanks. Wish you merry Christmas. |
This contribution was helpful to1 thankful Users |
Follow us on