1/11/2011 1:23 PM | |
Posts: 23 Rating: (0) |
Hello Dear, Led light is SF-DP on my plc. My CPU model is 315-2AF00-0AB0. I am start learning Siemens so i don't know about profibus yet. Currently i am using stand alone ( no network interface ), Dear. i follow your instruction and attached file. Please kindly take a look and guide me. thanks! Bgrds, pmm AttachmentDiagnose.zip (1138 Downloads) |
1/14/2011 3:00 AM | |
Joined: 10/7/2005 Last visit: 4/18/2024 Posts: 3003 Rating: (1046)
|
Hello phyoemaung your 315 is quite an old model and I presume thatit does indeed have a dedicated "SF-DP" LED over and on top of the "SF" and "BUSF" LED's and that only this "SF-DP" LED is lit, correct? If so (and I'm going ourt on a limb here), I believe the lit "SF-DP" LEDis simply a result of the non-configured Profibus DP interface. As such - and while annoying - it will not give you any problems (you do NOT use the DP port). To get rid of thelit "SF-DP" LEDthough, please try the following: 1.) Open up HWconfig and double click on the DP port of your CPUwhich will bring up its properties window. 2.) Click on the "Properties" button in the center of the popup window (in the "Interface" frame) to open up the properties of the Profibus Interface. 3.) Click on the "New" button to create a new Profibus network which is now assigned to the CPU's DP port. 4.) "OK" all the popups (you should now see a Profibus Master system line in HWconfig coming from the CPU's DP port). 5.) Compile & Save HWconfig 6.) Download HWconfig tothe CPU Even though you will NOT have any DP Slaves on the Profibus Netwrok, the DP port is now configured and your "SF-DP" LEDis (hopefully) off. I hope this helps and please let us know how it went. |
Cheers |
|
10/14/2016 10:56 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4775 Rating: (123) |
New question published by kero2016 is split to a separate thread with the subject Delete node in profibus from the hardware configuration. Best regards |
10/15/2016 7:12 PM | |
Posts: 142 Rating: (2) |
Which CPU u r using??? |
Follow us on