4/14/2020 11:04 PM | |
Joined: 7/28/2018 Last visit: 8/29/2022 Posts: 9 Rating: (0) |
Hi all, I have a similar project with connection only by Profinet.Two separate control cabinets for two machines with S1200 PLC and KTP700 panel each. Now I need to do 3rd control cabinet that had only HMI (the same KTP700) with all visualization cloned from two main control cabinets and control both PLC with R/W posibility. All system is in the same IP subnet. 1. How to clone two HMI all information to one HMI (maybe there's easy way to do that)? 2. I think to put into this HMI one more main page to choose between one machine PLC to another PLC control. How organize all three HMI synchronization? 3. How to arrange control, that from two HMI one PLC could be controlled and each HMI be updated? Any info are welcome. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/15/2020 10:42:21New subject after splitting |
|