8/8/2019 1:26 AM | |
Joined: 4/29/2015 Last visit: 8/20/2024 Posts: 2 Rating: (0) |
But if it´s always activated there why can´t be possible configure WinCC 7.4 with a PLC 1200 with firmware <= 3.x, or the communication with them have to be done with OPC server necessarily? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/08/2019 07:05:08New subject after splitting |
|
8/8/2019 3:19 PM | |
Joined: 9/27/2006 Last visit: 9/19/2024 Posts: 12282 Rating: (2684) |
Hello Joaquin; MisTsc is correct, you do not use PUT and GET functions for a connection with WnCC v7.4, you need the "S7-1200, S7-1500 channel", based o Profinet tolink a S7-1200 to WinCC. You can see examples of this type of configuration between a S7-1200 v2,2 and WinCC v7.4 in the following document: WinCC Connection to S7-1500, S71200 and ET 200SP https://support.industry.siemens.com/cs/ww/en/view/101908495 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 08/08/2019 15:20:53 |
|
Follow us on