11/7/2014 7:56 AM | |
Posts: 12 Rating: (0) |
Hello guys, i need help on how to connect the CU310-2 PN via LAN by using STARTER software? thank you for your help.
|
11/7/2014 9:15 AM | |
Joined: 5/12/2006 Last visit: 4/24/2024 Posts: 22226 Rating: (2980)
|
Hi, use accessible Nodes in STARTER to see which IP is activ on your CU! Regards Christoph |
11/7/2014 9:39 AM | |
Posts: 12 Rating: (0) |
Hi ChristophD, thank you for the reply. I did the Accessible nodes, and the result as shown in the picture below. is it like that? thank you. |
11/7/2014 10:11 AM | |
Joined: 5/12/2006 Last visit: 4/24/2024 Posts: 22226 Rating: (2980)
|
Hi, yes is see. only the Starter include Drives are listed, so you have installed no SSP. You can Download SSP an actual Starter here. and here. And Note: In your Project you have created a CU310 PN, not a CU310-2 PN ! Regards Christoph |
This contribution was helpful to1 thankful Users |
11/7/2014 10:22 AM | |
Posts: 12 Rating: (0) |
Thank you for your help, ChristophD. I try to install this software first and get back to you if I have problem with it. |
Follow us on