8/18/2017 8:32 AM | |
Joined: 4/24/2006 Last visit: 4/26/2024 Posts: 8615 Rating: (1147)
|
Hello phuoc, You can use the USB-PPI multi master cable to upload OP77A, using Prosave. See the following link: Which connector cables are available for connecting to SIMATIC Panels? In Posave, select in tab General, the panel OP77A and connection: 'Serial (via USB/PPI cable' Best regards, Wizard |
8/18/2017 9:36 AM | |
Joined: 4/24/2006 Last visit: 4/26/2024 Posts: 8615 Rating: (1147)
|
Hello phuoc, Sorry, my mistake You should choose PC/PPI cable Properties: Local connection: USB Best regards, Wizard |
8/18/2017 9:45 AM | |
Posts: 16 Rating: (0) |
it is not work, what is the number that I should input for address at properties tab? |
8/18/2017 10:02 AM | |
Posts: 16 Rating: (0) |
Hi, It is still not work. I want to know how to set the value of address ppi of Hmi, I can't find it out. |
8/18/2017 10:25 AM | |
Joined: 4/24/2006 Last visit: 4/26/2024 Posts: 8615 Rating: (1147)
|
Hello, Here is a manual: SIMATIC HMI HMI device OP 73, OP 77A, OP 77B (WinCC flexible) See chapter 6 Be sure the Serial channel is enabled. And is HMI panel in transfer mode Best regards, Wizard |
Follow us on