11/13/2015 12:25 PM | |
Posts: 23 Rating: (0) |
Hi Is there have any methods to online a simotion through Ethernet with scout? what should i do ? |
11/13/2015 1:02 PM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980) |
Hi, look at this FAQ: https://support.industry.siemens.com/cs/ww/en/view/22016709 From the Thread Topic and the not existing question: VPN Connection between the two cities must be exist. Connect the Simotion to the Ethernet Router which is connected to internet and configured for the VPN On you site start the VPN Client and establish a VPN Connection to the Router in the other city ping the ip of the simotion if this works go online inschout and do what you want.
Christoph |
This contribution was helpful to1 thankful Users |
11/17/2015 3:47 AM | |
Posts: 23 Rating: (0) |
Hi Christoph What i set with my router is display in attachment ,i hope you can read Chinese. Regards bobo |
11/17/2015 6:33 AM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980)
|
Hi, no i can't read chinese. Regards Christoph |
Follow us on