5/1/2020 10:51 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
I believe the string that you have comes from a list of materials you defined in batch. so, you could create a custom-made block, If string input is equal to string input in your defined input, send DINT as output. you could have 20 strings input named from ID1 to ID20, the DINT_IN1 to IN20. Then if String input = String ID5, send DINT ID5 out to Output. Hope it helps you. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to1 thankful Users |
5/1/2020 2:10 PM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926)
|
Hi, For this, I always use FC37: STRNG_DI that can be found at the Standard library->IEC functions->IEC. It converts a string (character size does not matter) to a DINT. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to2 thankful Users |
5/1/2020 2:42 PM | |
Posts: 3 Rating: (0) |
Yes you are right, for the Materials this would be a Solution. |
5/1/2020 2:43 PM | |
Posts: 3 Rating: (0) |
Thank you, I will take a look for the FC37 |
Follow us on