4/10/2020 6:56 PM | |
Posts: 66 Rating: (0) |
Hello Experts I am using VLVANL Block for giving commands to my analog output valves In the attached picture when i touch the item 0.5 it appears on the MV but the button 0.5 freezes any thing we can do to make this work without frezzing so that i can give 0.5 each time and icrease MV Value Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/11/2020 10:08:37New subject after splitting |
|
4/10/2020 10:26 PM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928)
|
Hi, it looks customized. So in order to debug the freezing, please do the following: 1. Browse to Windows Explorer to the following path: C:\Program Files (x86)\SIEMENS\WinCC\uTools and open apdiag.exe. 2. Click on: "Output Window" and report back the error that is shown when you press the button. Thx! PS: Create a new topic next time, the topic you responded to with your post has nothing to do with each other. Thx again |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
4/15/2020 1:13 PM | |
Posts: 66 Rating: (0) |
Hello Experts Please suggest as I am having still the same problem Thanks |
4/16/2020 9:18 AM | |
Posts: 66 Rating: (0) |
Hello Experts Please suggest as i am having the above problem Thanks |
4/16/2020 11:20 AM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928)
|
Hi, I have looked into the issue. I'm having V9.0 and direct control takes about a second to process, but no freezing. Since it works in V8.1 but not V8.2, I'm asking if you updated the library to V8.2 and did you update OS project editor? or are you still using V8.1 faceplates? Are the APL blocks as well as the faceplates the same version? V8.1 blocks with V8.1 faceplates etc,? Also did you change anything in the faceplate? particular the @PG_APL_OA_Analogwithlimits100.pdl? When the button is pressed (one of the four direct control buttons), a script is triggered called APL_AnalogPercent. What you can do is the following...if you are familiar with script handling. Open the C-script on the server under Global Script->C-Editor->Standard functions->APL->APL_AnalogPercent and in the script remove all the // signs that are in front of printf commands. Compile the script via the button right side of the little blue clock symbol and save the script. Open the apdiag.exe, open the output window and press the button and report back what is on the output window. After that place back the // signs in front of the printf commands to restore the script. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to3 thankful Users |
4/17/2020 8:40 AM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928)
|
Nice!!! I wonder what is was....will/can you share the old @PG_APL_OA file with me? I'm curious |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on