9/10/2016 12:42 PM | |
Joined: 1/21/2016 Last visit: 4/22/2023 Posts: 83 Rating: (1) |
|
Amr Ali |
|
9/11/2016 10:44 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, AS-i modules are connected to PLC CPU via CP. Is your present AS-i module is fully utilized? You must be checking cross references of input. If you could attach your project hardware here, more help about input identification could be provided. If the new input sensor, which you want to connect is quite away or if no spare input is available on the present AS-i module, you need to purchase AS-i module & needs to be modify your hardware & PLC logic. For more details about AS-i, visit this link & download the manual. HTH. |
Last edited by: PISCEAN 2010 at: 9/11/2016 10:51:27 AMLast edited by: PISCEAN 2010 at: 9/11/2016 11:10:44 AMAS-i manual link posted. |
|
9/11/2016 11:38 AM | |
Posts: 16 Rating: (0) |
Dear All, Thanks your help. But i still do not understand yet. So, could you read attached doc which i wanna ask? Thanks and Best Regards. AttachmentThis is my program.docx (67 Downloads) |
Follow us on