Industry Online Support
Technical Forum
11/14/2012 5:17 AM | |
Posts: 2 Rating: (0) |
hello all, I currently drive improvements 1200KW, with two parallel inverter attached. inverter current one we do not use because there are no spare parts, w017 alarm appears safe stop. how do we remove one inverter but does not appear warning and fault? corresponding manual which I read: 1. Jumper connection x9.5 and x9.6 2.Resetting drive definition (MLFB) at P70, but the warning persists and I find that the terminal does not exist, because the drive category of the old type. Thank you for your advise Attachmentdrive simovert.pdf (63 Downloads) |
11/20/2012 9:57 AM | |
Posts: 27 Rating: (1) |
if A017 appear you must check CUVC or VSB |
Follow us on