1/10/2023 6:44 AM | |
Joined: 6/7/2021 Last visit: 8/31/2024 Posts: 3 Rating: (0) |
Hi, have you find solutions of above probelm..? Actually I am also facing similar problem. |
1/10/2023 9:16 AM | |
Joined: 5/24/2016 Last visit: 9/13/2024 Posts: 347 Rating: (52)
|
Hello. On the 802D it was to my knowledge only possible to deactivate REPOSA if the Follow Up mode on the axis was disabled. Siemens has a topic to a similar problem in the knowledge base: Preventing REPOS in follow-up mode during part program processing. But normally one would do this change in the PLC using either M codes or other implementations. On the newer controls you can prevent the ASUP to run in MDI using MD20114 Bit: 0 - If this does not fit your application using MDI instead the solution is the same as in the link above. |
Follow us on