4/9/2018 8:20 AM | |
Posts: 3 Rating: (0) |
Dear Experts, Aveen ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/10/2018 9:32:12 AMNew subject after splitting |
|
4/10/2018 8:40 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Please attach existing DC motor name plate photograph. |
4/15/2018 6:09 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hello, Here I assume these DC motor are S1 duty & for main spindle application. If the application differs by duty cycle or if it is for crane application the motor may change or any other specific application, you need to study motor loading pattern & motor characterstic. For 400 HP motor you can use 1PH8356-1XH4X motor. For other motors e.g. 500, 600 & 800 HP motor, the rated torque is much higher i.e. > than 12000 Nm as these are low rpm high torque motors, so I suggest you to contact Siemens. Please refer the attached sheet for information. HTH. |
This contribution was helpful to1 thankful Users |
4/21/2018 6:13 AM | |
Posts: 3 Rating: (0) |
Thanks for the info.. |