2/25/2020 10:44 AM | |
Joined: 3/9/2018 Last visit: 4/16/2024 Posts: 179 Rating: (14) |
Bear in mind V3.1 is tended to be used on Windows 2000 SP2 and lower and might be very incompatible to be working with windows 10. Which version of STEP 7 Micro/WIN or S7-200 PC Access is compatible with which version of MS Windows? By upgrading the adapter to latest driver driver V3.1 might not recognize the adapter and/or old driver can not work with windows 10, hence the incompatibility. You can try different compatibility modes and/or play with the driver if needed. Recommend upgrade to the latest version V4.0.9.25 or use a virtual machine (VM) with Windows 2000 on it. V4.0.9.25 is officially not supported on Windows 10 but can work after some trial an error. (search topics) |
Last edited by: Henry1675 at: 02/25/2020 10:49:17Last edited by: Henry1675 at: 02/25/2020 11:13:19Last edited by: Henry1675 at: 02/25/2020 11:37:43Last edited by: Jen_Moderator at: 02/25/2020 14:33:22Optimized link. |
|
2/26/2020 9:36 AM | |
Posts: 7 Rating: (0) |
hi the laptop I was previously using is also a win 10 laptop from 2018. the one that i used to use worked perfectly with no modifications whatsoever. I dont think its a compatibility issue but rather a communications settings problem. I am just not sure what parameters i should alter |
Follow us on