3/15/2011 12:17 PM | |
Joined: 6/1/2007 Last visit: 2/15/2021 Posts: 33 Rating:
|
We have a system where in SIMOTION C (C230-2) is used for controlling four axes operation. However the system is running well. We have a project in SIMOTION Scout and we are also able to connect to the CPU but when online it shows that C230-2 and the axes and the programms are not there in the memory and we cannot monitor the parameters inside the CPU. In the project when online the C230-2, AXES and the program elements shows Red+Green Mark ahead of them. Splitted from Convert Word to Integer in S7. |
Last edited by: O_Moderator at: 3/15/2011 1:18 PMnew subject after splitting |
|
3/15/2011 1:19 PM | |
Joined: 4/24/2009 Last visit: 4/8/2021 Posts: 2693 Rating:
|
Thread closed, because question is already published in the following thread UPLOAD from SIMOTION C using SIMOTION SCOUT. Best regards O_M;oderator |
Follow us on