1/26/2015 8:30 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2145)
|
Hello Rashid29, You can try to use the "WinCCViewerIP Control", if this camera can send via TCP/IP. For more information see the former thread in the forum. /tf/WW/en/Posts/48203 Regards Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
11/25/2015 11:19 AM | |
Posts: 1 Rating: (0) |
Where is the MRL option? |
2/10/2016 11:05 AM | |
Joined: 6/26/2014 Last visit: 7/29/2022 Posts: 42 Rating: (2) |
And how to configure. (I'm not able to insert 2 attachments in one post) |
2/10/2016 4:32 PM | |
Joined: 12/28/2015 Last visit: 1/24/2024 Posts: 256 Rating: (26) |
Hello, it is so important that your camera have the option rtsp. Before I tested it in WinCC I have installed on the WinCC Server the program of the camera. So I checked that the network Configuration is right and I can see a picture. In the control I select the IP Adress and the Password. But I had a camera for Tia portal. There was another control but this FAQ helps me 62383298. Maybe it can help you to configure your camera. |
5/12/2020 8:33 AM | |
Joined: 6/19/2017 Last visit: 4/18/2024 Posts: 7951 Rating: (162) |
New question published by Poyo7070 is split to a separate thread with the subject Need to see some cameras through RTSP. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on