9/4/2018 4:52 PM | |
Joined: 11/17/2016 Last visit: 1/26/2021 Posts: 11 Rating: (1) |
Dear colleagues, can you possibly give me a hint how to install ALSA drivers for the purpose of using plug and play usb sound cards like in the case below which is related to Intel Galileo Gen 2. https://gist.github.com/cpmpercussion/0e731d25dd0825a30273 Is it possible to install the necessary ALSA package without the need of creating an own customed SD card image for IoT2040? Can you point out how to install additional Kernel modules in general in context of modprobe use ? Thank you very much in advance! ------------------------------------------------------------------------------------------ AttachmentHOWTO setup Pd on Intel Galileo · GitHub.pdf (112 Downloads) |
Last edited by: Jen_Moderator at: 9/5/2018 7:06:17 AMNew subject after splitting |
|
9/6/2018 4:21 PM | |
Joined: 4/28/2015 Last visit: 9/9/2024 Posts: 3345 Rating: (379)
|
Hi, I don't think that it is possible to run this without building a new image since there are kernel modules required. And on the other hand the tutorial uses opkg to install additional packages. The opkg packages are based on a old kernel version and outdated, so they may destroy your system. You can try to install the ALSA packages from source, but I can't say if this will work in the end. Keep us updated! Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
9/17/2018 12:10 PM | |
Joined: 11/17/2016 Last visit: 1/26/2021 Posts: 11 Rating: (1) |
Hi, I also think that your described approach with building a customized image could be more successful in here so I tried to follow the instructions under Modifying the SD-Card Image / Adding new Layers But also here I got into trouble unfortunately. I have described it under that topic instead here. Maybe you could have a look into the according message and maybe you could have a further hint for me what to try? Pleaseeee :-) |
Follow us on