7/29/2013 2:47 PM | |
Posts: 5 Rating: (15) |
To install STEP 7 v5.5 SP3 (DVD update release) follow these steps. 1. Download and install the latest 64-bit version of automation licence manager. http://support.automation.siemens.com/WW/view/en/114358 2. Copy DVD content to any directory on hdd. 3. Modify ./Setup.exe using any resouce modification software. Eg ResourceHack. Add the line <supportedOS Id="{4a2f28e3-53b9-4441-ba9c-d69d4a4a6e38}"></supportedOS> //this is the os ID of Windows 8 64bit 4. Modify ./InstData/Setup.ini under section OS. PlattformIDAllowed = 1;2;3 Add the lines Win8x64=1 5. Modify all msi-files to enable the ingore-button on installation failures (like installing on unsupported OS's). Use any software possible to manipulate MSI-files. E.g. InstEd. Search for DLG_INSTALLATIONREQUIREMENTS_DISABLE_IGNORE. Change Action from Disbale to Enable. Run ./Setup to start installation. Press the ingore-button when told it's not possible to install on running OS.Good luck! Disclaimer. I can not be held responsible to any result caused by following this guide. It's just for educational purposes. |
This contribution was helpful to21 thankful Users |
9/6/2013 11:48 AM | |
Joined: 9/11/2011 Last visit: 7/10/2023 Posts: 52 Rating: (0) |
Thanks friend |
1/5/2014 11:56 AM | |
Joined: 1/28/2009 Last visit: 1/22/2022 Posts: 21 Rating: (0) |
Dear sir I need more explanation. because i can't follow your method and i still can't install it thanking you |
3/21/2014 12:42 PM | |
Posts: 1 Rating: (0) |
hello i'm be so happy if you learn us with picture to how do this rule you said in this post. tnx |
4/7/2014 10:01 PM | |
Joined: 1/12/2010 Last visit: 12/18/2023 Posts: 5 Rating: (0) |
can you give us more explaination with photo |
4/12/2014 12:48 PM | |
Posts: 1 Rating: (0) |
you can not tell me more? if any pictures are great too! thank you! performed in step 4 how so?
|
6/23/2014 10:30 PM | |
Posts: 4 Rating: (0) |
I just recieved the same error. I am attempting to uninstall and re-install Step 7 ... crossing my fingers. |
6/30/2014 4:37 PM | |
Posts: 2 Rating: (0) |
I didn't understand where I should add these lines. Can you please,explain more with some screen shots ? |
6/30/2014 4:38 PM | |
Posts: 2 Rating: (0) |
I didn't understand where I should add these lines. Can you please,explain more with some screen shots ? |
9/23/2014 9:05 AM | |
Posts: 1 Rating: (0) |
Dear JonasBentsson, Can you guide step by step? I'm using Windows 8.1, I use Resource Hacker software but I don't known "add the line support windows 8.1" and modify msi files. Thanks.
|
Last edited by: WhiteTiger at: 9/23/2014 9:06 AM |
|
10/20/2014 10:59 AM | |
Joined: 1/28/2013 Last visit: 4/22/2024 Posts: 37 Rating: (8) |
Brother its not working i cant installing on windows 8.1 can you help me..? |
Follow us on