5/26/2019 5:28 AM | |
Posts: 59 Rating: (0) |
Hi, I have problem with Digsi 4.86 which is installed after installation of Simatic Manager Step 7 V5.5; Clicking Digsi 4.86 causes opening of Simatic Manager with all options for PLC and Siprotech Devices such as 7SJ61, 7SJ62 etc. is possible to add under device. But plug and play option is not available here whereas this plug and play option is available when only Digsi is installed. Under PLC, plug and play option is showing inactive. Can anyone advise how to make plug and play option active in my digsi which is installed along with Simatic Manager Step 7 V5.5 ? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/27/2019 12:20:05New subject after splitting |
|
5/27/2019 10:01 PM | |
Posts: 59 Rating: (0) |
After changing view from component view to topological view, it is working fine. Thanks |
Follow us on