12/21/2010 5:11 AM | |
Posts: 41 Rating: (0) |
Hi guys, Any body tell me how to mask (or) Bypass the fault temporarily. |
12/21/2010 6:50 AM | |
Joined: 8/25/2006 Last visit: 9/19/2024 Posts: 2209 Rating: (278) |
Look at parameter P830. |
12/22/2010 7:20 AM | |
Posts: 41 Rating: (0) |
Hi KSN, how P830 works? |
12/22/2010 8:16 AM | |
Posts: 41 Rating: (0) |
If i want to mask the fault number F013, then what can i do in P830. |
12/22/2010 9:00 AM | |
Joined: 8/25/2006 Last visit: 9/19/2024 Posts: 2209 Rating: (278) |
Enter 13 in parameter P830. |
12/22/2010 9:12 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181)
|
OFFTOPIC! And what is meaning of F013? |
Follow us on