Industry Online Support
Technical Forum
11/8/2013 4:59 PM | |
Posts: 40 Rating: (0) |
.
Attachment2.pdf (428 Downloads) |
11/8/2013 5:02 PM | |
Joined: 7/7/2010 Last visit: 9/18/2024 Posts: 15204 Rating: (2417)
|
OB_NR is just the Number part of the OB right? In this case, 200, not OB200. |
science guy |
|
11/11/2013 2:53 PM | |
Posts: 40 Rating: (0) |
Great! Thank you, it was my mistake
I think I've solved the two things that you indicated but OB200still does not work .. AttachmentDocumento1.pdf (382 Downloads) |
11/12/2013 2:23 PM | |
Joined: 9/8/2009 Last visit: 7/17/2023 Posts: 1410 Rating: (152) |
Attach and detach are to be used only at pulse (event, ...) whenever you want to add or remove it, not to be executed every scan cycle. You also have an error of exeuction of attach function. Maybe if you search the forum you will find others that succeded to make interrupts working. In some links I have found there is either no mention the need to attach interrupt, I guess if you configure it in configuration it shall attach and enable automaticly when you dowload the program /tf/WW/en/Posts/90763 Compile everything and download to PLC, check your connections, monitor the input that has to trigger interrupt, do you see input changing state?It has to be a minor problem for sure. |
Follow us on